Other Parts Discussed in Thread: INA4230, INA4235
Tool/software:
Using this part, sometimes it is difficult to place the monitor close to the current/voltage source you wish to monitor, especially with a 3 channel device such as this.
The data sheet recommends placing the current sense resistors close to the INA3221 (in my case 10m-ohm 1W), but what if the current needing monitoring is "further away" from the 3221? Wouldn't it be better to place the current sense resistor close to the thing being monitored and run the 2 traces (IN+ & IN-) back to the 3221 in order to reduce the high current resistance path so as to obtain best accuracy?
Or might it be better to just keep the current sense resistor close to the 3221 as the data sheet recommends but then run thick traces from the thing being monitored back to the current sense resistor and 3221.
Thoughts?
Thanks!