Kindly help me in selecting TI's N-channel JFET with following specs:
1. Regulator threshold:
MIN: 4.5V
TYP: 4.75V
MAX: 5V
2.VGS(off) ; MIN: 1.5V
MAX: 4.2V
3. Vol at drain pin will always 3<=Vin<=10
Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Kindly help me in selecting TI's N-channel JFET with following specs:
1. Regulator threshold:
MIN: 4.5V
TYP: 4.75V
MAX: 5V
2.VGS(off) ; MIN: 1.5V
MAX: 4.2V
3. Vol at drain pin will always 3<=Vin<=10
Regards
Hi, Deepak,
Are you looking for a discrete JFET device? If so, I don't believe TI makes any such device.
-d2