Tool/software:
Hi,
the Operating junction temperature for LM231N is -20°C to 80°C. Is there a wider operating junction temperature version of LM231N? such as -40°C to 125°C
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ken,
Is there a wider operating junction temperature version of LM231N? such as -40°C to 125°C

These are all legacy IC, and we do not have the industrial operating range in these. LM2917 and LM2907 are also V-to-F converters, but they are limited to 85C as well, due to RC time constant conversion topology.
https://www.ti.com/lit/SNAA088
What is your application?
Best,
Raymond