This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-3PHGANINV: Minor correction in documentation

Part Number: BOOSTXL-3PHGANINV


Tool/software:

Hi,

I am working with the BOOSTXL-3PhGaNInv board at present, and would like to report the following corrections in the user guide:

File: sluubp1a.pdf

Link: https://www.ti.com/lit/pdf/sluubp1

 

  1. Pp#7, Section: 2.2: J6 should be renamed to "J5" as there is no "J6" on the BOOSTXL-3PhGaNInv EVM. The jumper J5 is the only jumper available on the EVM. (There was one J6 with TIDA_00913 but that's a different version.)
  2. Two warnings on the same page advising to remove J6 when C2000 Launchpads are connected should be updated to mention J5.

 

Request you to update the changes when time permits.

--

Darshankumar Pandit