Part Number: INA228
Tool/software:
Hi,
I currently have the problem, that I don't know if the values I send to any register on the INA228 are saved correctly or not.
When I try for example to write 0x9000 to the ADC_CONFIG_REGISTER, the chip acknowledges the values. When I then try to read the value from the ADC_CONFIG_REGISTER I can only read 0x22FF, which should be impossible because the bits 3-0 are reserved and always set to zero.
My question is: Am I doing something wrong with the writing or the reading process?