Part Number: THS2630
Tool/software:
Hi,
I am using three THS2630 ICs to convert signals to differential voltages, which are then sent to the ADC.
My Vcom is set to 2.048V, and the power input is ±14V.
During testing, I ground the input pin, both VOUT- (pin #5) and VOUT+ (pin #4) measured 2.048V.
After powering on, I noticed that the current draw from my power supply is high (0.14A) compared to a PCB without the THS2630 (0.04A). Additionally, the temperature on the surface of the IC is quite high, around 60~70°C.
Using a multimeter to check the diode voltage on each pin of the IC, I found that VOUT- only has 0.4V, while the rest of the I/O pins are all above 1V.
Is this behavior normal for this IC?
According to the datasheet, the quiescent current should be a maximum of 13.2mA.
I have attached the electrical schematic of the THS2630 section.
I would appreciate any advice. Thank you!
Adam Shiau