This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2904: Need a EOL year for MPN: LM2904AVQDRQ1

Part Number: LM2904


Tool/software:

Hi,

We need a EOL year and availability for this MPN:  LM2904AVQDRQ1

  • Hello 

    LM2904AVQDRQ1 consists of LM2904, Q1, D package, and low Vos which has no foreseeable end. Many decades likely.

    I recommend using this orderable part number LM2904BAQDRQ1 instead.

  • Hi,

    Thanks for your reply

    If no plan for EOL ( LM2904AVQDRQ1) , can we consider it is active in another 10 year 

    and can you provide the difference between LM2904AVQDRQ1 and LM2904BAQDRQ1 .......Is that any major changes in parameters

  • Balaji,

    Yes may may consider it is active in another 10 year. No major changes in parameters, meaning what happen in normal operation.

    For non-normal operation, for example both inputs above VCM range or any input below VCM range, LM2904AVQDRQ1 will have more variable results than LM2904BAQDRQ1. The "B" version is newer fab process so there are modernization advantages with that.