Tool/software:
Hi, I'm testing the circuit below and it's detecting the AC peak instead of zero cross, unless I connect oscilloscope to isolated GND OUT2 then it works as expected.
Is connecting Neutral to INN necessary or can it be floating.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi, I'm testing the circuit below and it's detecting the AC peak instead of zero cross, unless I connect oscilloscope to isolated GND OUT2 then it works as expected.
Is connecting Neutral to INN necessary or can it be floating.

Hi LA,
Yes, this makes sense.
I think you may need to consider a change in architecture in order for the circuit to work properly.
Building something like this is an option: https://www.ti.com/lit/an/snva735/snva735.pdf
Or using a standalone DC/DC converter to convert voltage from the low to the high voltage domain is another.
An example of such a circuit can be found on the EVM, we also have modules from TI: https://www.ti.com/power-management/acdc-dcdc-converters/overview.html