Part Number: INA143
Tool/software:
|
Subject:
INA143 |
|
From:
Jack Frost - Summit Products <summus@summitproducts.com> |
|
Date:
10/1/2024, 11:53 AM |
|
To:
"Featherstone, Chris" <cfeatherstone@ti.com> |
This circuit should have a gain of 100 (2 stages) if I'm correct. WHAT AM I DOING WRONG?
The measured voltages at U2 are:
PIN VOLTS
1 1mV
2 0.9mV
3 2.7mV
4 2mV
5 2.71V
6 2.71V
7 4.99V
8 N/C
Regards,
Jack