Tool/software:
Dear Team,
I was going through this article from TI regarding Unused opamp termination. It says that when Opamp is single supply you can use the termination given in below figure.
Figure 1:

When it is working Split Supply Rail(Assuming Symmetric) you can use the termination given in
Figure 2

My question is regarding split supply operation.
When the split supplies are not equal,Let V+ be 15V and V- be -13.5V. In this case which termination scheme is good ?.
I believe in this case the termination scheme given in Figure1 is good because it will reduce the
current draw by the opamp from the supply.Please correct me if I am wrong
Regards