Part Number: TIPD191
Other Parts Discussed in Thread: INA128, OPA188
Tool/software:
I am studying TIPD191 Instrumentation Amplifier with DC Rejection Reference Design recently, it's a inventive circuit. I have some questions about this circuit.
Is OPA188 and INA128 together forming a negative feedback loop to keep Vref consistent with offset of Vin? I think there is a loop between Vref and Vout.

Below is integrator circuit of opa188 and simulations, a pole and a zero appear in curve of vin, frequency of pole is about 1.59Hz, which is created by R1 = 100k and C3 = 1uF, frequency of zero is about 3.27kHz. I don't konw which compoents cause this zero, at frequency of 3.27kHz, impedence of C3 is about 50ohms, considering inverting amplifier formed by R1 and C3, 20*log(50/100k)=-66dB, this value is same to flatten area of high frequency above 3.27kHz of vin. So why does curve of vin become flat in high frequency?