Part Number: INA823
Other Parts Discussed in Thread: INA826S
Tool/software:
I would like to use INA823 to monitor the voltage of an attached battery.
If the whole circuit is powered off, the connection to the battery is still there and therefore the circuit sees 0V at -IN and 3.7V at +IN,
which usually causes some current from +IN to V+ to sort of back-power the whole circuit, which I need to prevent,
but the main question therefore is: are those overvoltage FETs turned off and therefore prevent a current flow (if within ±5V) at +IN and -IN when the circuit is powered off?
I attached a picture of how the external and internal circuit roughly looks like: