Part Number: OPA836
Tool/software:
1.First, the operation amplifier circuit test conditions: VDD voltage DC3.6V, S IN input signal suspended in the case.

2. The test waveform at each point is as follows: The waveform at ① is as follows:

②The waveform is as follows:

③The waveform is as follows:

④The waveform is as follows:

3. Questions and how to improve (1) Why are the waveforms at (1) and (2) different, why are the waveforms at (2) cluttered? (2) In the case of input suspension, there is a signal at ④, how to solve it? (3) How can this circuit be improved to normally amplify the input 300KHZ, the amplitude of 10mV signal, and the output amplitude of 1V after amplification?