Part Number: INA241B
Tool/software:
What are the internal REF1 and REF2 resistor values? I need to estimate reference source loading.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA241B
Tool/software:
What are the internal REF1 and REF2 resistor values? I need to estimate reference source loading.
They are matched, but an absolute value is not specified or guaranteed.
Section 8.4.3.4 says:
The reference pins are designed to be connected directly to supply, ground, or a low-impedance reference voltage. The reference pins can be connected together and biased using a resistor divider to achieve a custom output voltage. If the amplifier is used in this configuration, as shown in Figure 8-8, use the output as a differential signal with respect to the resistor divider voltage. Use of the amplifier output as a single-ended signal in this configuration is not recommended because the internal impedance shifts can adversely affect device performance specifications. If single-ended measurement is required, TI recommends to use an external op amp to buffer the resistor divider voltage (see Figure 8-9).
Hello Valued Engineer,
I am looking this over and will respond shortly.
Sincerely,
Peter
Hello,
REF1 and REF2 resistors are typical 50 kΩ at +/-20% absolute value variation as Clemens referred to. The actual matching tolerance error between these two resistors is specified in the datasheet.
Sincerely,
Peter