This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2188: OPA2188 运放内部的静电absorpion device启动的条件

Part Number: OPA2188


Tool/software:

在官方视频讲解图中,运放模型内部有一个吸收电路如下图absorpion device,问题1:请问这个是晶闸管电路吗

下面以OPA2188 标准跟随电路,同相输入,正端串联输入电阻,供电电压为±15V,运放输入信号为-14V~14V DC。

在电路上电工作中,为了防止外部EOS,比如浪涌差模试验2KV(1.2/50us),在运放输入正端输入串联电阻阻值 10K(考虑精度希望阻值在合适范围内尽量小降低噪声)的功率电阻,瞬态电流达到200mA,时间:几十us

是否会触发运放内部absorpion device启动(我们不希望上电状态下启动),造成运放的电源短路烧坏

问题2:那么这时候内部的absorpion device触发的条件:电压 是否为Absolute Maximum Ratings ±18V? and 电流是多少?

知道电压方便选择外部供电引脚的TVS钳位电压

知道电流方便选择 运放正端输入限流电阻(这里指的不是运放内部静电二极管持续稳态电流10mA),而是absorpion device的瞬态触发电流,

除了增加运放输入正端的串联电阻,选用一个PPTC串联在运放供电﹢15V,限制电流在60mA以内,是否absorpion device启动了,也能有效防止运放烧坏? PPTC参数如下: