Part Number: TLV7011
Tool/software:
Hello,
I have the circuit in the picture

The output of the comparator is connected to series resistor of 100kOhm and then to OR gate.
I need to make PWM with time period of 10 seconds and ON time of 0.5 second.
I have a problem that when the output is high (3.3V), and the non inverting input pin is 2.2V, the inverting input pin charges and the output toggles to low before the inverting pin reaches 2.2V:

Blue - inverting input pin
Yellow - non inverting input pin
As you can see, sometimes it reaches to 2.2V and sometimes not.
The problem above is happening only if i connect the output of the comparator to OR gate via 100k ohm series resistor. If the output of the comparator isn't connected to anything the problem disappear
What is wrong?
Thank you
Maor M.