Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA190: High-side current source

Part Number: INA190
Other Parts Discussed in Thread: OPA187

Tool/software:

I need to create a high-side DC current source which will be adjustable from 100-1000uA. The supply rail is 5V.

The plan is to use a Precision DAC for setting the reference (IN+) of a Precision Op-Amp, and closing the loop (IN-) with a shunt resistor and INA190:

Rshunt = 100R

INA190 G=25

VDAC = 0.025-2.5V --> 100-1000uA

Amp is probably OPA187

Do you have any guidance on this application? 

Thanks