Part Number: OPA2187
Tool/software:
The output of some amplifiers changes by about 1.4 mV at temperatures between 20 and 30 degrees Celsius.
During testing, the operation changed when the resistance of the op-amp was changed to 200 kΩ, 820 kΩ, and 51 kΩ, so I think that the change in input bias current may be the trigger.
I also think that the input bias current may be changing due to temperature changes, so I would like to hear your opinion on this.