Tool/software:
Hello
I am using Pspice .lib file as a circuit model in Cadence for using it in a type III compensation system I use the model as it is but I feel there is a lot of extraneous code in the pspice model file.
For the following circuit:
I am expecting a response as this:
The above response is typical for a type III compensator with phase boosting
As soon as I insert the OPA323 model:
I get a very unexpected open loop gain and phase plot with both the phase and the gain starting from a negative valued scale:
Is the code for the pspice model correct. WHat needs to be done or edited in it. I just need to use the OPAMP as it is and then compensate it using my values