Part Number: TPS61288
Tool/software:
Hi,
I am using the Boost converter module TPS61288 to generate 9.0V from battery source whose typical voltage is 7.4V and it may range from 5.8V to 8.4V. The discharge capacity of the battery is 7.5A peak current and 1A continuous current. The current drawn by the load is 6.2A during surge and 0.8A during continuous operation.
I have attached the schematic for the reference, please confirm if the schematic is good to go
And also confirm if pulling the Enable pin to low will disable the output completely or still Vout=Vin like in most of the boost converter modules. In my application, I need to turn off the 9V output completely when not is use. If the enable on pulled low will disable only the set output voltage and still the Vin will be seen on the Vout pin, I need to implement a separate logic for turning off the Vout completely, please confirm
Thank you