Part Number: VCA810
Tool/software:
Hello,
I have a question concerning the VCA810 Wideband and Variable Gain Amplifier that I use as a Log Amplifier from -40dB to 40dB gain.
According to the datasheet, the component has an VOLTAGE_OUTPUT_SWING = +/-1.8V (3.6Vpp) for Vc=-2V and RL=100Ohms.
I control 10 different gains thanks to Vc from -2V to 0V, and for every gain test, I am almost at +/-1.7V, which is suitable. But for my X1 gain, I have poor results. The ouput is limited and +/-1.1V...So almost 600mV away of the real limit. As in Figure 1 bellow, for VIN=1.80V (yellow), VOUT=1.05V (purple).
FIGURE 1
The other probleme is for the gain accuracy. Except for gain X1, for every gain, the output saturation is at almost +/-1.8V, but the gain is not very accurate, for acheiving 1.8V at the ouput for a we need more than 180mV for gain X10, more than 18mV for gainX100, etc. For example, if my VIN=1.8VPP, I have differente results if my signal is centered according to 0 or if it is between 0V and 1.8V as we can see in Figure 2 and Figure 3 : 

FIGURE 2 FIGURE 3
Indeed, this is due to an "early limit" in the output swing I guess. But this means that the gain is only accurate bellow a certain value of VIN (under 500mV for example)...
Some theories are suitable then :
- For the limit problem at +/-1.1V for gainX1 : maybe the teeple point? Vc control unstability?
- For the gain accuracy : same limit output swing problem?
I have a 25Ohms resistance at Vc pin to the ground, a 50Ohms resistance in series at the ouput pin to adapt.
Thank you for your help.
Best regards.









(example from different device)