This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA296A: if GND pin can connect to -0.3V

Part Number: INA296A


Tool/software:

According to datasheet of INA296A, the linear range of the output stage swing to Ground is limited to 20mV(max). Seems it can not detect current less than 4mA if  using gain=50 and external shunt resistor=0.1ohm. circuit as below, If connect the gnd pin to -0.3V, i think it will detect current less than 4mA. So I want to know if the GND pin can connect to -0.3V and what would be the impact of that.