Other Parts Discussed in Thread: OPA992, OPA2992
Tool/software:
Hi,
I have designed a charge amplifier that requires IEPE type output.This IEPE circuit requires a constant current source for power supply.
When the current value is 8mA, it works normally. The DC output voltage should be 2.5 * 4.433=11.08V.
But in reality, sometimes the output is about 1.9V when powered by a 4mA current source. When powered by an 8mA current source, everything is normal.
Once the output is 11V, it will remain stable and work normally. Once the output is 1.9V, it remains abnormal.
The schematic diagram is shown below(P1 is connected to IEPE input, and P2 is connected to charge output):