This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1311: Absolute max question

Part Number: AMC1311

Tool/software:

Hello,

I am using the AMC1311B and i put 2V at the input and the supply of the IC can be turned off. In the datasheet i saw that i cant place above VCC+0.5V at the input. Is it ok to place 2V at the input (when VCC=0) while i draw less than 10mA with series resistor?

Thank you