Other Parts Discussed in Thread: TLV906X
Tool/software:
Hi team,
This is from the optical module suppliers requirement. They need to design 120Khz, 3mA peak SINE waveform which can be adjustable. I think that there will be 2 parts. The first part is used to generate SINE waveform while the second part is used to convert voltage to current. So as below picture, do we have any formula to calculate the amplitude and frequency. The customers need to adjust them. Is there any possibility to only adjust amplitude, such as adding some signal? If convenient, could you please also help give a simulation as reference?