Other Parts Discussed in Thread: LM117,
Tool/software:
I have 28V (nominal) input to the LM117, and the output is adjusted to 16V. Please advise on the following:
1. If 1Vrms (frequency 50kHz to 400MHz) is input on top of the 28V input power supply during EMC testing, will the output be 16V without any malfunction?
2. Can a voltage in the range of 21V to 33V be operated at frequencies from 50kHz to 400MHz?
3. Is it possible that the output voltage will fluctuate due to noise?