Other Parts Discussed in Thread: THS4552
Tool/software:
Dear TI,
could you please extend the CMRR and PSRR curves in the datasheets of THS4551 and THS4552 to 100MHz? The end is at 10MHz at 85dB (CMRR) and 80dB (PSRR, 5V). I need the values up to about 30MHz, 100MHz would be nice.
Under the curve is written: "simulated with G =1 V/V" (CMRR) and "simulated to differential output". Can I trust that these CMRR PSRR values are reached in the real usage of THS4551 or THS4552?
Thanks!
Merten