This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA692: OPA692 AC-coupled drive

Part Number: OPA692

Tool/software:

Hi,

Need to drive analog PAL video over 5 meters coaxial cable, therefore it looks like capacitive AC-coupling is required.

The question is if the OPA692 can drive the 75R coax load via large serial capacitor?

  • Hi Eli,

    The device should have no problem with AC coupling at the output assuming the other end of the signal is properly terminated to 75ohms. However, I am unsure about the 1K resistors at the output. I am not too familiar with this configuration. As for the values of the coupling capacitors, we often recommend values significantly larger (330uF) to limit any potential discharging affects. 

    Best Regards,

    Ignacio

  • Thanx, Ignacio.

    I understand that amplifiers with SAG input minimize that capacitor by factor of 10?

  • Hi Eli,

    That is the benefit of implementing some kind of sag correction circuitry. There are devices that have this functionality and use values in the same range, but I am unsure how effective the configuration shown is with SAG correction when implemented on PCB. 

    Best Regards,

    Ignacio