Tool/software:
Hi, I'm in the process to design a headphone amplifier, as part of a hifi preamplifier. I thought this could be based on the OPA551, which I see is widely available. I see the performances are impressive.
My requirements are:
- single power supply available (28 Volt), about 80-100mA per channel
- balanced input
- capability of the integrated circuit body to be easily heatsinked (like the OPA551 in TO-263 case), as I'm always concerned about reliability - temperature. This for example made me exclude the TPA6120A2DWP, another interesting option
- little bit of gain, about 2 in the example
- capability to drive 16 to 600 Ohm headphones
- as the power supply is somewhat limited to 2.5 Watt per channel, I'm not interested to the ultimate in terms of sound pressure, a good 200mW would be more than enough.
This is the design I defined, I'd like to ask your opinion with regards to: stability, and utilization of single supply (as you can see I've biased the two input signals at 14V, with 3.9K precision resistors. It means 3.5mA additionally drawn, I'm fine with that).

thanks so much in advance
A good day
Matteo