Part Number: PGA855
Other Parts Discussed in Thread: ADS8900B, THS4551, THS4541, THS7001, , LMH6629, PGA870
Tool/software:
We would like to use the PGA855 to directly drive an AD9653 16-bit ADC running at 20 MSPS. The maximum frequency of the signals is 1 MHz sine wave.
The PGA855 makes the statement that it can only directly drive ADC with sample rates up to 1 MSPS. I need help understanding the limitation.
Why does the PGA care about the ADC sample rate? What is the reason for that limitation?
And the PGA855 datasheet claims to have a bandwidth of 10 MHz.Even at 1 MHz bandwidth, a 1 MSPS ADC is pretty low and would only be good for a couple hundred KHz. What is the point of having a PGA with 10 MHz bandwidth if you can only use it up to say 200 KHz?