This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA994: The relationship between output current ability and power supply

Part Number: OPA994
Other Parts Discussed in Thread: OPA593, OPA690

Tool/software:

Hi team,

I see that OPA994 can output 120mA in the datasheet. But it also depends on the power supply. So my question is that if the power supply is 10V, the output voltage range is 4~10V and output current range is 32~100mA. Can OPA994 support this requirement? Could you help check it or do the test to verify whether it can support this requirememnt?