Part Number: ISO224
Other Parts Discussed in Thread: AMC3302, AMC1300
Tool/software:
Hello, good morning.
I am trying to design a power quality analyzer that senses line voltage and current, and detects transients, harmonics, peaks, frequency, apparent and reactive power, among others.
I wanted to know if this device would be suitable for this application.
The idea is to sense 300VAC from the line, reduce this voltage to a value below 12V (which is what the ISO224 input supports) using resistors, and then add a follower on the output to get an ADC input from 0 to 3.3V.
I understand that the ISO224 gain is 0.333, so with a 12V input, I would get almost 4V on the other side, correct?
My question is that in all the diagrams I've seen, there’s a low-pass filter on the input. Could I remove this filter in my design? Because I actually want to capture line imperfections on my ADC. Also, at what speed should I sample with my ADC?
Any information or diagrams would be very helpful.
Thank you very much for your help.