This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XTR106: ESD rating

Part Number: XTR106

Tool/software:

What are the ESD ratings for the XTR106? Both HBM and CDM. Thanks!

  • Hi David,

    Great question! I can provide what I've seen a few devices survive, but please understand this isn't TI guaranteeing that all devices will be able to handle these HDM and CDM levels. It's possible not all devices will be able to handle this. This is to just give you a better idea of how robust the XTR106 is. 

    HDM - 4000V

    CDM - 750V 

    Best Regards,

    Robert Clifton