Part Number: LMV761
Other Parts Discussed in Thread: TLV3201
Tool/software:
Hello,
I would like to know if it can be guaranteed, that the LMV761 (LMV761MFX/NOPB to be concrete) does not go into phase reversal if one of the inputs exceeds the common mode input voltage range, while still being inside the maximum input voltage range? In my application the other input would always be within the input common mode range.
For instance:
The amplifier is supplied with 3.3V, hence an input common mode voltage range according to the datasheet of 2.0V.
One input is fed by a ramp signal ranging from 0V to the supply voltage, while the other is at a steady voltage below 2.0V.
The comparator output is expected to trip when the voltage of the ramp signal exceeds the voltage of the steady voltage. What happens when the ramp signal goes above the CMVR of 2.0V? Does the output remain stable or may there be a inverted phase at the output?
Unlike the TLV3201, which specifies NO phase reversal even if the inputs go beyond the supply voltage, the LMV761 does not specify anything.