Other Parts Discussed in Thread: OPA846, OPA657
Hi,
Please find the op-amp requirements below:
The desired features (in order of importance) are as follows:
- First stage gain of 400-500K (more the better)
- Low input bias current (pA, hopefully fA level)
- Low noise
- Single Supply (hopefully something that works with 3.5V or so)
- Rail to Rail (not a huge requirement)
I have looked at OPA846 and OPA657.
Would like to check if there are other recommendations.