Tool/software:
Hi team,
Could it allow AC input between HVin and LVin?
Regards,
Ochi
Hello Ochi,
The short answer is yes it is usable but for low frequencies. The RES60-Q1 is optimized for DC and low frequency applications. We don't have data for AC measurements and some of the specs are TBD. For now I can say the bandwidth is shown below from the PDS. I released an EVM for the device as well.
https://www.ti.com/tool/RES60EVM
Best Regards,
Chris Featherstone
Hi Chris
Thank you. Considering several hundreds of kHz bandwidth, It looks suitalbe for 50Hz / 60Hz, 200V AC signal. Any other concern for using this device for AC signal? For HV pin, it will have ±200~300V referring to its LVIN pin, is it OK?
Regards,
Ochi
Hi Ochi,
I do not see an issue using an AC signal with the conditions you described. Let me know if I can be of further assistance.
Best Regards,
Chris Featherstone