This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XTR110: Current Loop, Multiple Devices

Part Number: XTR110

Tool/software:

Hello , 

If I have multiple XTR110s in a system, and I have a shared power supply which means the ground is common to each channel, should I return the low-side of the load in the current loop back to pin 2 (common) directly to the respective device to avoid shared loops ? I have seen some older systems that have a shared loop between two devices which connect at a single ground point and then branch off to pin 2 of each device. In my mind avoiding shared loops would be ideal. Any advice would be much appreciated. Thanks.