Part Number: LM358
Tool/software:
I required op-amp output delay minimum 5 sec with dwell channel op- amp IC/ CKT
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM358
Tool/software:
I required op-amp output delay minimum 5 sec with dwell channel op- amp IC/ CKT
Hi Piyush,
The LM358 is a dual op-amp with 1.2-MHz BW. Sorry, I don't quite understand the question. LM358 amplifier itself will typically have a response much faster than 5s; but will need more information to put this question into the right context:
What sensor or signal source circuit is being measured? what is the output load or circuit connected to the amplifier output? What are the supply requirements? What input voltage signal amplitude or DC voltage is being measured, input common-mode and frequency?
If you can kindly provide a preliminary schematic or block diagram of your application circuit, this will be helpful.
Thank you and Kind Regards,
Luis