This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS7376: Is it suitable for 50m VGA cable application?

Part Number: THS7376


Tool/software:

Hi Team,

My customer is surveying solution for supporting 50m cable VGA display application.

Could you please advise whether THS7376 is suitable for such scenario to enhance driving strength?

Thanks.

Best regards,

Terry

  • Hello Terry,

      A couple questions are needed to determine if the device is suitable:

    1. What is the total load customer needs to drive with the amplifier? Especially important if customer needs to drive a high capacitive load.      



    2. Will they impedance match?
    3. What is customer's expected output voltage range? 
    4. What is their input frequency?

    Thank you,
    Sima