Other Parts Discussed in Thread: INA229, SYSCONFIG
Tool/software:
Hi TI Experts,
I am going to use INA229 for my power management system. I am now testing the INA229 using INA229EVB. I am using Microchip SAMD51, every things is ok such as reading/writing registers and getting Vbus, except the current reading are incorrect. So, to make it simple and easy, I am now evaluating using an Arduino UNO. Here is the snapshot of the configurations (default), CHIP_ID = 2291, Manufacture_ID= 5449, noted that Vbus is read properly.
(WITHOUT R_SHUNT connected) I have tried to apply voltage to IN+ and IN- to read V_SHUNT, I apply around 145mV and others, It reads properly:
Then to measure/evaluating the current, I connect the R_SHUNT of 1 mili ohm and apply the same V_shunt voltage around 145mV:
The Vshunt and current are the same value which is also wrong. It happens also when I use microcontroller SAMD51. In addition, I have also calculate the shunt_cal and program it as in Datasheet.
Best regards,
Fajar