Part Number: INA105
Other Parts Discussed in Thread: INA2132, INA132
Tool/software:
I am using a 6-axis load cell which has a built in amplifier. However, the output signal is differential and the analogue inputs I am using are single ended.
Therefore I need to convert the differential signal to single ended.
I was wondering if I could use an INA105 Precision Unity Gain DIFFERENTIAL AMPLIFIER to convert the differential signal to single ended and if so how ?
Details about the load cell are below (M3815C) :
- https://www.srisensor.com/m38xx-series-6-axis-ft-sensor-for-low-capacity-high-product/
- https://www.srisensor.com/uploads//M3815C.pdf
The supplier provided the following example of the differential signal: "+signal" is 3.5V, "-signal" is 1.5V, thus the common mode is (3.5+1.5) / 2 = 2.5V and the input voltage is (3.5-1.5) = 2V.
Alternatively are there existing off the shelf devices that will convert differential to single ended ?