Tool/software:
Dears,
Recently, the current monitoring of INA226 in the customer's radar equipment failed. The current value read was fixed at 8192mA, and the actual value should be within 20mA. After replacing the new INA226, the data was read normally, and the current value was still 8192mA after re-welding, which ruled out the problem of cold soldering. The chip appearance was not damaged, and the function was good when it left the factory. Can the problem of current error caused by the damage of pin 9 be reduced by improving the circuit?
Best Regards,
Arabella Zhang