Other Parts Discussed in Thread: OPA4990, OPA4170, TLV9304, TLV4170, ADS7028, LM7705, TLV9061, TLV9302
Tool/software:
Dear,
We wrote to check the issue as below, U3 and U5 are powered by +24VDC, for the U3, we add a + 1.25V to the + port, and the Vout seems right, but as for U5, we connected the +port to the GND, and the output of the U5 is not right when the input is very low. Is it the reason for this issue is the OPA(U3/U5) which we selected is not rail to rail? If yes, Would U like to recommend us a high precision, rail to rail, 4 channels, low speed application OPA? Thanks.