Other Parts Discussed in Thread: INA500,
Tool/software:
In the following circuit:
What would be the expected variation of VF1 with variation in VS2 from 1.8 to 3.6V and across temperature?
We are seeing a change in this especially at -40 deg.C.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Ashvin,
I tried to replicate this effect. I saw virtually no change with temperature. How much did you see, please show the data and the Tina circuit.
There is gap between 1.8V and 3.6V, but no line slope with temperature.
Hello Ron,
We saw this change in a circuit we rigged up. The input to this opamp is from an INA500 (VS1). The circuit seems to be giving the right output at higher VS2 but at VS2 of 1.8V, the output starts off at the desired value of 600mV but starts to drift upwards with respect to time. This happens only at -40 deg. C.
Also if we look at the model of the TLV8812, it does not show any dependence of the PSRR to temperature. What else could be causing this change in the output at low voltages and low temperature?
Ashvin,
Does this happen on more than one sample of TLV8812? Can you provide specific data? Does this drift stop after the op amp has soaked sufficiently; no longer changing temperature on the inside.
Yes, this happens on at least 4 samples. the drift stops after the opamp has soaked sufficiently.
Ashvin,
At cold, condensation could create a leakage path that could affect the output voltage. Other than that, the unspecified magnitude drift would be normal for TLV8812.
Ashvin,
Why is 30k a minimum, where does this come from?
minimum of 30K resistance at the output?
In the schematic snippet, there is no closed loop for U2B
Section 7.4.4 Driving Capacitive Load states that there could be oscillations due to a capacitive load and the output impedance of the amplifier.
Ron,
We had an issue with instability in the PI controller, now that is resolved by making the loop slower.
Thanks for the support.