Part Number: LF353
Tool/software:

We currently use the LF353DR operational amplifier for amplifying differential signals. We have tested the differential signal input at 0.127V and amplified it by 1.8 times. The calculated single ended signal should be 0.2286V, but the actual measured output is 0.251V. The magnification factor is about 2. After replacing the LF353DR purchased 22 years ago. The magnification is normal. May I ask if there are any process updates after 2022 that may cause changes in certain parameters?