Other Parts Discussed in Thread: PGA280
Hi All,
I am planning to measure -ve and +ve voltage on my board using PGA280 amplifier.
If I use VSP=+15V , VSN=-15v, VSOP=5V and VSON=0V( GND) ( Fig 43 in PGA280 datasheet)
and G=1 what would be the differential output voltage range for the following inputs.
Vin = +10V , 5V , 0V , -5v , -10V.
what would be the range for VOP and VON for all the above input , if I use VSOP=5v. and output signal rate ?
from the data sheet , its not clear on diffrential output range of the device.
Can I interface PGA280 out to an ADC with diffrential input capability with signal range of 3.3v ?
please help.
thanks.