Tool/software:
Dear Specialists,
My customer is considering PGA870 and has questions.
I would be grateful if you could advise.
---
(1) I am considering using the DVGA PGA870 as a front-stage amplifier for an AD converter (ADC3223IRGZR). Can I use it?
There is no reference circuit for DC input, but can I use it without any problems with DC?
Could your please provide a circuit example.
(2) On page 18 of the data sheet, Single-Ended to Differential Operation, it says:
" If a single-ended signal source is to be dc-coupled to the device, its voltage swing should be centered about the midsupply reference, VMID1. If the input dc voltage is greater than 0.2 V from midsupply, then increased distortion and reduced performance can result. The non-driven input pin of the PGA870 should be ac-coupled to ground through a capacitor. In this configuration, the PGA870 amplifies the difference between the dc-coupled input signal and the midsupply reference. "
Does this mean that the input voltage is limited to ±0.2V around VCM when DC-coupled?
---
I appreciate your great help in advance.
Best regards,
Shinichi