Part Number: OPA858DSGEVM
Other Parts Discussed in Thread: TDC7201
Tool/software:
Dear TI:
I recently bought your OPA858DSGEVM and want to use it with TDC7201 to conduct laser ranging experiments, but some problems have occurred. The output of my APD is shown in the first picture. The 1064nm beam is used and the maximum level output reaches 1.48V. I refer to the data sheet and the user manual. When I use a single power supply input, VCC uses 5V, and VEE is grounded, the output is only more than 200mv. When using dual power supplies VCC3V and VEE0.8V, the output is only 320mv. This does not conform to the principle that it can amplify 7 times in phase. Is there something wrong with the product I bought? I have read all the posts about OPA858DSGEVM in the forum and tried VCC+2.5V, VEE-2.5V, but it still doesn't help. I hope the engineer can reply to me after seeing it. Thank you. My project is very urgent.