Other Parts Discussed in Thread: INA116, INA118, INA333
Hi all,
I have done some experiments with the INA116 and could not understand some of the phenomenons. I was trying to understand the common-mode rejection capability of the IA. I have tried three different configurations and the schematics are as below. I was using a signal generator to produce a 32kHz sine wave with amplitude of 200mV. The gain of INA116 is set to 10.
In scenario A, the ground of the signal is connected to the ground of the INA116. The output signal is good as expected. In scenario B, I purposely made sure that the ground of the signal from signal generator is not connected to the ground of the INA116. As INA116 is a differential amplifier it should be able to amplify the difference, which is the signal although the grounds are not shared between two systems. However, the output is very wrong. I see very big noise and very unstable signals shown as below.


In scenario C, I was connecting two grounds with a 1Meg resistor to simulate when two systems grounds are not well connected together. The result is same as scenario B.
So my questions are:
1. Is there are something wrong with the IA so it is not able to amplify the difference between two inputs and disregard the common mode voltage?
2. Or is there something wrong with my test methods? What shall I do if I want to amplify some differential signal whose reference could be not connected to IA ground?
Thanks indeed.
Best Regards,
Jianglei