Other Parts Discussed in Thread: ADC12DL1500, TINA-TI
Tool/software:
Hi team,
I am using LMH5401 for driving the ADC12DL1500.
Will this drive the S to D conversion with maximum efficiency?
Our steady state voltage is 0.8V with +/-400 mVpp. The Vcm is 0V for ADC12DL1500.
I have tried simulating LMH5401 in Tina-Ti.
My Input:
DC Voltage = 0.8 V, G=1, No Input Termination.
Peak to Peak Voltage = +/- 400mVpp

My Output: 
Why am I not getting sharp edges in rise and fall time? Please give me solution to rectify the error and rise/fall time in the output.
Do I need to add or reduce any compensation for this?

Thanks
Aashik S